Extension Manager
Menu Path:
The tab provides a way to select which extensions are loaded during VSA startup. Types of extensions include measurement extensions (LTE, 802.11n/ac, etc.), hardware extensions, and processing extensions.
When the check box next to a measurement extension is selected, the extension will be loaded when the VSA is started. When the check box is cleared, the extension will not be loaded.
You will need to restart the 89600 VSA software after making changes.
You can reduce memory usage by clearing the check boxes next to the extensions that you do not need. Startup time will also be reduced.
Clicking on a measurement extension title will provide the following information:
- Created by: indicates the author of the extension
- Description: short description of what the extension does
- Version: version of the extension's .NET assembly (.dll)
VSA Extension Manager Application
The extension manager can be run as a separate application in addition to running within the VSA. To access the application, use this path:
Extension Manager Configuration Files
With the application, you can create multiple configuration files. This is useful if you want to start multiple instances of the 89600 VSA, each with different sets of extensions loaded.
Default Configuration File
On startup, the 89600 VSA attempts to read an xml-formatted file that specifies which extensions to suppress loading. This file is located here:
%USERPROFILE%\My Documents\Keysight\89600B VSA\20xx\ExtensionManager.xml
where 20xx is the version of the 89600 software.
This file does not exist until you have used the Extension Manager.
This is the file that is loaded by default when you run the application.
Command-line
To specify which extension manager xml file to load when starting the 89600 VSA, use this syntax:
Agilent.SA.Vsa.Vector.exe /extensionmanager:"c:\path\to\ExtensionManager.xml"
Agilent.SA.Vsa.Vector-x64.exe /extensionmanager:"c:\path\to\ExtensionManager.xml"
The tab will edit the Extension Manager xml file that was loaded when the VSA was started. When no Extension Manager file is specified, the VSA will edit the Default Configuration File (see previous section).
Menus
The following are the menus provided by the :
-
-
- loads the xml file that you specify for editing
-
- saves the changes to the currently loaded xml file
- - saves the current xml file to another filename
- - exits the application
-
-
-
- accesses this topic
-
See Also